SPRUJ79A November 2024 – December 2025 F29H850TU , F29H859TU-Q1
The DEBUG_CFG register controls the authentication method used to control debug access at the C29DBGEN level and each of the user ZONE debug levels. For each debug access control, there are two valid configuration options:
The DEBUG_CFG register has LOCK/COMMIT protections to prevent unintended or unauthorized changes to the debug authentication scheme. To lock or commit these settings, write to the DEBUG_CFG_LOCK and DEBUG_CFG_COMMIT registers as required.
The current debug status for C29DBGEN and each of the user debug ZONEs can be determined by connecting to the SEC-AP interface and reading the DEBUG_ENABLE_STATUS register. For more details, see the SEC-AP gel file, which contains a script to read the DEBUG_ENABLE_STATUS register. GEL files are located in the following CCS installation directory: C:\ti\ccs_version\ccs\ccs_base\emulation\gel.
Devices shipped from the TI factory have password-based authentication active at boot-up by default. To change the startup debug authentication mode, update the DEBUG_CFG field in the SECCFG sector accordingly.