SPRUJD3A July 2025 – October 2025 F28E120SB , F28E120SC
In addition to the prefetch mechanism, a data cache of 128-bits wide has been implemented to improve data space read performance. This data cache is separate from the instruction prefetch buffer, and is used for data reads only. Whenever a data read access is performed by the CPU to a Flash bank address, if the data located at that address is not presently loaded into the data cache, then the Flash wrapper reads 128 bits of data from the Flash bank and stores the data in the data cache. This data is eventually sent to the CPU for processing. The starting address of the Flash bank access is automatically aligned to a 128-bit boundary, such that the requested address location is within the 128 bits to be read from the bank.
The data cache is disabled by default
at reset. To enable the data cache, set the DATA_CACHE_EN bit in the FRD_INTF_CTRL
register, or call the Flash_enableCache() driverlib function. Note
that the data cache gets bypassed when RWAIT is set to zero.