SPRUJD3A July 2025 – October 2025 F28E120SB , F28E120SC
FILE: sci_ex3_echoback.c
This test receives and echo-backs data through the SCI-A port.
A terminal such as 'putty' can be used to view the data from the SCI and to send information to the SCI. Characters received by the SCI port are sent back to the host.
Running the Application Open a COM port with the following settings using a terminal:
The program will print out a greeting and then ask you to enter a character which it will echo back to the terminal.
Watch Variables
External Connections
Connect the USB cable from Control card J1:A to PC