SPRUJD3A July 2025 – October 2025 F28E120SB , F28E120SC
FILE: sysctl_ex1_missing_clock_detection.c
This example demonstrates the missing clock detection functionality and the way to handle it. Once the MCD is simulated by disconnecting the OSCCLK to the MCD module an NMI would be generated. This NMI determines that an MCD was generated due to a clock failure which is handled in the ISR.
Before an MCD the clock frequency would be as per device initialization (160Mhz). Post MCD the frequency would move to SYSOSCDIV4.
The example also shows how we can lock the PLL after missing clock, detection, by first explicitly switching the clock source to SYSOSCDIV4, resetting the missing clock detect circuit and then re-locking the PLL. Post a re-lock the clock frequency would be 160Mhz but using the SYSOSCDIV4 as clock source.
External Connections
Watch Variables