SPRUJD3A July 2025 – October 2025 F28E120SB , F28E120SC
Figure 15-38 shows the architecture of the PWM Crossbar (X-BAR). This module enables selection of various trigger sources into any of the dedicated MCPWM trips inputs.
Figure 15-38 PWM X-BARThe PWM X-BAR has eight outputs that are routed to each MCPWM module. Figure 15-39 represents the architecture of a single output but the output is identical to the architecture of all of the other outputs.
Figure 15-39 PWM X-BAR Architecture - Single OutputFirst, determine the signals that can be passed to the MCPWM by referencing the PWM X-Bar Mux Configuration Table (see Section 9.2.1.1). Select up to one signal per mux (32 total muxes) for each TRIPx output. Select the inputs to each mux with the TRIPxMUX0TO15CFG and TRIPxMUX16TO31CFG registers. To pass any signal through to the MCPWM, enable the mux in the TRIPxMUXENABLE register. All muxes that are enabled are logically ORed before being passed on to the respective TRIPx signal on the MCPWM. To optionally invert the signal, use the TRIPOUTINV register.