SPRUJD3A July 2025 – October 2025 F28E120SB , F28E120SC
SYS_ERR consolidates several sources of interrupts (see Figure 3-3). These sources set the respective bit in the SYS_ERR_INT_FLG register. Any set bit in the SYS_ERR_INT_FLG register also sets the global interrupt (GINT) bit. The GINT bit has to be cleared before any SYS_ERR interrupt is generated. If the GINT bit is cleared with the source flags still set, another SYS_ERR interrupt is signaled; therefore, clear the source flags before clearing the GINT bit. For System Error sources, please refer to SYS_ERR_INT_FLG register.
Figure 3-3 System Error