SPRUJD3A July 2025 – October 2025 F28E120SB , F28E120SC
The Comparator Subsystem (CMPSS) consists of analog comparators and supporting circuits that are useful for power applications such as peak current mode control, switched-mode power, power factor correction, voltage trip monitoring, and so forth.
See the C2000 Real-Time Control Peripheral Reference Guide for a list of all devices with modules of the same type, to determine the differences between the types, and for a list of device-specific differences within a type.