SPRUJH0B April 2025 – September 2025
When plugged into a USB host, the XDS110 enumerates as both a debugger and a virtual COM port. J101 allows the user to connect the SCI UART from the F28E12x to the debug probe to be passed on to the USB host. By default, the F28E12x SCIA maps to the virtual COM port of the XDS110 using GPIO35 and GPIO37. See Section 2.1.3.2 for limitations.
To enable SCI boot on the F28E12x LaunchPad, follow the below steps:
Refer to Serial Flash Programming of C2000 Microcontrollers for additional information on utilizing the SCI bootloader.