SPRUJH3 April 2025 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280023 , TMS320F280023C , TMS320F280025 , TMS320F280025C , TMS320F280034 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037C , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039C , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041C , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049C , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377S , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1 , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
If the user needs to boot to code already programmed in the on-chip flash, then users can either use the default BMSPs to boot to flash entry point address 0x0008 0000, or configure the BOOTPIN-CONFIG and BOOTDEF registers to boot to a specific flash address.
The default BMSPs to configure boot to flash can be found in the TMS320F280015x Real-Time Microcontrollers data sheet. If the user sets both GPIO24 and GPIO32 to 1, then the boot ROM branches to flash entry address 0x0008 0000 without needing to configure the device registers.
However, if users need to boot to a different flash sector, then the BOOTCONFIG and BOOTDEF registers need to be configured for the specific boot option. Refer to the GPIO Assignments section in the data sheet to find which boot option to configure to reach the intended flash entry point. These steps describe how to emulate boot to flash entry point 0x0009 0000. For example, boot option 0x63.