SPRZ412L December   2013  – June 2020 TMS320F28374D , TMS320F28375D , TMS320F28376D , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28378D , TMS320F28379D , TMS320F28379D-Q1

 

  1.   1
    1.     2
    2.     3
    3.     4
    4.     5
      1.      6
        1.       7
        2.       8
        3.       9
        4.       10
      2.      11
    5.     12
  2.   13
  3.   14

Caution While Using Nested Interrupts

Revision(s) Affected:0, A, B, C

If the user is enabling interrupts using the EINT instruction inside an interrupt service routine (ISR) in order to use the nesting feature, then the user must disable the interrupts before exiting the ISR. Failing to do so may cause undefined behavior of CPU execution.