SPRZ439H January 2017 – February 2024 TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
Figure 2-1 and Figure 2-2 provide examples of the F28004x device markings and define each of the markings. The device revision can be determined by the symbols marked on the top of the package as shown in Figure 2-1 and Figure 2-2. Some prototype devices may have markings different from those illustrated. Figure 2-3 shows the device nomenclature.
Figure 2-1 Examples
of Device Markings for PM and PZ Packages
Figure 2-2 Example of Device Markings for
RSH Package| SILICON REVISION CODE | SILICON REVISION | REVID(1) Address: 0x5D00C |
COMMENTS(2) |
|---|---|---|---|
| Blank | 0 | 0x0000 0000 | This silicon revision is available as TMX. |
| A | A | 0x0000 0001 | This silicon revision is available as TMX. |
| B | B | 0x0000 0002 | This silicon revision is available as TMX and TMS. |