SSZT201 january 2021
Bluetooth® Low Energy is on a path to become ubiquitous. The Bluetooth Special Interest Group estimates that by 2024, all new phones, tablets and laptops will support Bluetooth Classic and Bluetooth Low Energy. They also expect 35% of devices to ship with single-mode Bluetooth Low Energy by 2024, which represents 300% growth in annual shipments.
The reason for this is the versatility of Bluetooth Low Energy. Bluetooth Low Energy continues to expand its capabilities to meet new applications. Features including LE audio, mesh, positioning services and many more have been added to adapt to the growing demand in applications such as asset tracking, health and fitness, Internet of Things, access control and more. Due to its versatile capabilities and widespread use in smartphones which enables interoperability and immediate deployment in existing systems, Bluetooth Low Energy is becoming the go-to standard for a variety of automotive applications.
Recent trends suggest that automotive manufacturers are embracing Bluetooth Low Energy for tire pressure monitoring systems (TPMSs), cable replacement, telematics, wireless battery management systems, personalization, smart wearables and LE Audio. Let’s explore a few of these applications.
Stand-alone Bluetooth Low Energy is a single chip capable of performing Bluetooth Low Energy only.
From a connectivity standpoint, it’s possible to achieve a better power budget by adding a stand-alone Bluetooth Low Energy node in the head unit or telematics box that acts as a wakeup source for the entire system. Once a smartphone or key fob comes into range, the node sends a wakeup signal that turns on the other wireless systems on the vehicle.
Beyond power savings, using a stand-alone Bluetooth Low Energy chip has these advantages:
Most TPMSs use two separate integrated circuits (IC) – a low-frequency radio IC and an ultra-high-frequency IC. The downside is that this method requires the vehicle’s central processing unit (CPU) to use a separate, dedicated receiver for both wireless technologies, requiring maintenance of each.
Alternatively, we could design the TPMS nodes with Bluetooth Low Energy only, which offers long range support and power efficiency that allows for higher robustness and longevity as well as native support in smartphones which allows for excellent interoperability between the vehicles other Bluetooth Low Energy systems. Moreover, TPMS can be incorporated as part of a Bluetooth Low Energy network in the vehicle.
By using smart and efficient design, designers can save costs by combining multiple applications on a single Bluetooth Low Energy node. For example, since the vehicle’s main CPU already includes Bluetooth Low Energy, you can leverage this node to act as a data collector for the TPMS, increasing efficiency and reducing the total amount of wireless nodes in the vehicle, which in turn saves total system costs and increases node interoperability.