SSZTBP9 january   2016

 

  1.   1
  2.   2
    1.     3

Zachary Richards

As discussed in the previous post in this series, generating DC currents of arbitrary magnitude is a simple and straightforward process using op amp feedback and a voltage reference. However, suppose it was necessary to generate some arbitrary number (N, for example) of current sinks (or sources) each with its own arbitrary magnitude; perhaps to bias the various stages of some complex analog circuitry. While the reference voltage generation only requires a single implementation, repetition of the entire feedback portion of the sink could become cost- and design area-intensive. So a question emerges: Is it possible to implement such a bias network using a single feedback source? The answer is yes—though it gets somewhat complicated and certain conditions must be met—and this network (sink only for this analysis) is shown in Figure 1 below.

GUID-0A6BD93A-F018-4748-9A90-B91AA537C458-low.png Figure 1 Current Sink Network

Ultimately the source voltage of the MOSFET, VS, and the RSET resistor determine the sink current in each leg; by removing the feedback from the outer sink legs (that is, for all N > 1), direct control of VSN has been lost. Thus, RSETN must be carefully selected to generate the desired, arbitrary Nth leg sink current, ISINKN. Examining Figure 1 above, an equation can be readily derived which defines the ratio of the current in the Nth leg of the bias network to that of the first:

GUID-73E3C6A0-A7A9-4D06-8DFB-AD664E30BD55-low.png

Rearranging Equation 1 in to solve for the R1 to RN resistor ratio, MRN, yields:

GUID-4545CAEA-437D-45F7-8DDC-DFDAC39B777B-low.png

So what is the MOSFET source voltage in the Nth leg of the bias network, VSN? Consider the drain current equation for an NMOS operating in the saturation region:

GUID-20135273-4327-4175-A94B-D3A9AC2AD612-low.png

It is important to note that the effects of channel width modulation can be largely ignored here. This is because any increase in drain current from an increasing drain voltage would drop across the RSET resistor and result in an increased source voltage. In order for the MOSFET to maintain any current whatsoever, the gate voltage must be larger than the source and threshold voltages combined. That is, for a fixed gate voltage, the source voltage is ultimately clamped to at least a threshold voltage drop below it, and no amount of drain voltage increase will increase drain current. Therefore, establishing the operating condition that RSET must be sufficiently large to ensure this clamping allows the following assumption to be made:

GUID-3368C397-35F2-440A-BD00-1AC48FF448EA-low.png

The ratio expressed in Equation 5 can now be rewritten based on Equations 3 and 4:

GUID-E0D9D861-D1F8-4B42-A72A-E968E9C0B149-low.png

In order to simplify Equation 5, the following term can be defined:

GUID-9F565D50-D364-4B46-A047-3652D5415FED-low.png

After making this substitution and rearranging terms in Equation 5, an equation for VSN can be derived:

GUID-7314F179-9B4E-48CE-AF02-9DFE056E302A-low.png

Substituting Equation 8 into Equation 9 yields:

GUID-4C457303-0C5B-4FF8-B11E-05CECB927EAA-low.png

So what is the gate drive to threshold voltage difference, VGT? This is ultimately determined by the feedback in the first leg of the bias network; it is essentially the voltage required to maintain the desired ISINK1 current:

GUID-883733C8-1516-48E9-B40D-CD7A8BB933B2-low.png

After rearranging terms in Equation 11, an equation for VGT can be determined:

GUID-A3A47893-E7B3-4C10-B2FD-1DA4A91B9BB4-low.png

Substituting Equation 13 into Equation 10 yields:

GUID-46511D29-D671-490C-A4A6-1744BCBDD75E-low.png

Finally, the resistor ratio MRN can be written as a solely a function of MIN (along with some physical constants of the bias network devices) as follows:

GUID-31E09CAA-292F-4F0B-AA4D-D973572E3200-low.png

Now that an equation modeling the RSET resistor ratio has been derived; it’s implications on producing a bias current network with arbitrary magnitudes can be explored—the topic of the next blog in this series.