SWCU195A December 2024 – May 2025 CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755R10
Channels can be set up to perform software transfers through the DMA.SOFTREQ register. If the channel used for software is also tied to a specific peripheral, the dma_done/interrupt signal is provided directly to the Arm®Cortex®-M33 CPU instead of sending the signal to the peripheral. The interrupt used is a combined interrupt, software µDMA interrupt, for all software transfers.
If software uses a μDMA channel of the peripheral to initiate a request, then the completion interrupt occurs on the interrupt vector for the peripheral instead of occurring on the software interrupt vector.