SWCU195A December 2024 – May 2025 CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755R10
The PMCTL subscriber has six programmable events in the AON event fabric, which are ORed together to form a single wake-up event to PMCTL configurable through the EVTULL.WKUPMASK register. This wake-up event is used to trigger the wake-up of the MCU power domain from Standby mode. Any of the events listed in Table 4-7 can be chosen as input by selecting the appropriate event publisher or publishers. By default, this register is set to 0, meaning that no publishers are selected to drive the wake-up event towards PMCTL.