SWCU195A December 2024 – May 2025 CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755R10
In AUTO mode, the sample signal is generated synchronously to the sampling clock (SAMPCLK), and can be programmed using an internal sampling timer to determine the duration of the sampling window. The sample timer is 10 bits wide, and there are two sample time compare registers (SCOMPx) available to account for various source impedances from which to measure signals. One of these two SCOMP registers can be selected using the STIME bit in the MEMCTL register.
Figure 21-2 shows the ADC sample and conversion timing diagram when the ADC is configured in AUTO sampling mode.