SWRA466D February   2015  – August 2021 CC1310 , CC1310 , CC1352R , CC1352R , CC2538 , CC2538 , CC2620 , CC2620 , CC2630 , CC2630 , CC2640 , CC2640 , CC2640R2F , CC2640R2F , CC2640R2F-Q1 , CC2640R2F-Q1 , CC2642R , CC2642R , CC2642R-Q1 , CC2642R-Q1 , CC2650 , CC2650 , CC2650MODA , CC2650MODA , CC2652R , CC2652R , CC2652R7 , CC2652R7 , CC2652RB , CC2652RB , CC2652RSIP , CC2652RSIP

 

  1.   Trademarks
  2. 1Introduction
  3. 2ROM Bootloader
    1. 2.1 Configuring the Bootloader
      1. 2.1.1 CC2538
      2. 2.1.2 CC26x0
    2. 2.2 CC26x2
    3. 2.3 Communication Protocol
      1. 2.3.1 ACK/NACK
    4. 2.4 Interface Configuration
      1. 2.4.1 Hardware Pins
      2. 2.4.2 UART Configuration
      3. 2.4.3 Establishing Communication
      4. 2.4.4 Status Command
  4. 3Serial Bootloader Library (SBL)
    1. 3.1 SBL Return Values
    2. 3.2 SBL API
      1. 3.2.1 Device-Specific Functions
  5. 4Example Project
    1. 4.1 Hardware Setup
      1. 4.1.1 SmartRF06EB Virtual COM Port
        1. 4.1.1.1 External Serial Interface
      2. 4.1.2 LaunchPad Virtual COM Port
      3. 4.1.3 Bootloader Backdoor
    2. 4.2 Software Setup
      1. 4.2.1 Device Type
      2. 4.2.2 Baud Rate
    3. 4.3 Program Flow
      1. 4.3.1 Enumerate COM Ports
      2. 4.3.2 Create Device
      3. 4.3.3 Connect
      4. 4.3.4 Erase Flash Range
      5. 4.3.5 Write Flash Range
      6. 4.3.6 Calculate CRC32
      7. 4.3.7 Reset
  6. 5References
  7. 6Revision History

Hardware Setup

The SBL communicates with the ROM bootloader over a serial COM port on the PC. If a built-in COM port is not available, a USB-to-serial interface can act as a virtual COM port.

Figure 4-2 demonstrates two different ways to connect the PC to the device: one is using a level shifter to convert the UART signal from RS232 to TTL signals and the other is using a USB-to-UART bridge similar to what is used on the SmartRF06EB [4].

GUID-04753182-85A1-4904-9154-77CBE8A73134-low.gifFigure 4-2 PC to UART Connection