TIDUEU6B September 2020 – December 2021 OPA810
The circuit instability issue is resolved in the existing architecture with the help of compensation capacitor CF in parallel with RF as shown in Figure 2-5. The required value of CF also varies with unknown capacitance CX. Hence, it becomes impossible to find single value of CF which can stabilize the circuit for complete range of ZX.