DLPU102B December 2020 – July 2022
This section covers how to add pattern images and a batch file to the firmware. These steps allow the user to add patterns to the flash and have them automatically uploaded to the DLPC900 upon power up. The GUI is not connected when starting this process.
These steps generate a new firmware image containing the pattern images and batch file located in the pattern mode tab and the batch file tab respectively. This firmware file is ready to be uploaded to the system when connected. If the user desires to load a previously created batch file, ensure that the batch file begins with a DISP_MODE : 0x03 command and ends with a PAT_START_STOP : 0x02 command in order to have the pre-stored patterns run upon start-up.
An alternate method is to build a firmware adding only the images. Then add the batch file that updates the LUT and runs the images.