DLPU102B December   2020  – July 2022

 

  1.   Read This First
    1.     Trademarks
    2.     About This Guide
    3.     Related Documentation from Texas Instruments
    4.     If You Need Assistance
  2. 1DLP LightCrafter Dual DLPC900 EVM Overview
    1. 1.1 Welcome
    2. 1.2 DLP LightCrafter Dual DLPC900 Evaluation Module (EVM) Hardware
    3. 1.3 EVM Board
    4. 1.4 Other Items Needed for Operation
    5. 1.5 DLP LightCrafter Dual DLPC900 Connections
      1. 1.5.1 DLP LightCrafter Dual DLPC900 LED Enable and PWM Outputs
      2. 1.5.2 DLP LightCrafter Dual DLPC900 Trigger Input and Output Voltage Selectors
    6. 1.6 DLP LightCrafter Dual DLPC900 EVM Flex Cable
    7. 1.7 DLP LightCrafter Dual DLPC900 EVM and DMD EVM Assembly
  3. 2Quick Start
    1. 2.1 Power-up the DLP LightCrafter Dual DLPC900 EVM
    2. 2.2 Creating A Simple Pattern Sequence
  4. 3Operating the DLP LightCrafter Dual DLPC900 EVM
    1. 3.1  DLP LightCrafter Dual DLPC900 Control Software
    2. 3.2  PC Software
    3. 3.3  System Common Controls
      1. 3.3.1 Operating Mode
      2. 3.3.2 Connected DMD Type
      3. 3.3.3 EVM Information
      4. 3.3.4 Status
    4. 3.4  System Settings
    5. 3.5  Video Mode
      1. 3.5.1 Video Support
    6. 3.6  Pattern Modes
      1. 3.6.1 Menu Bar
      2. 3.6.2 Creating a Pattern Sequence in Pattern On-The-Fly Mode
      3. 3.6.3 Creating a Pattern Sequence in Pre-Stored Pattern Mode
      4. 3.6.4 Reordering a Pattern Sequence using the Edit LUT Feature
        1. 3.6.4.1 Special Considerations for Input Triggers when using the Edit LUT Feature
      5. 3.6.5 Creating a Pattern Sequence in Video Pattern Mode
      6. 3.6.6 Creating a Pattern Sequence With DMD Block Load
      7. 3.6.7 Pattern Settings
    7. 3.7  Batch Files
      1. 3.7.1 Execute Batch File
      2. 3.7.2 Creating and Saving Batch Files
        1. 3.7.2.1 Creating and Saving a Batch File Using the GUI
        2. 3.7.2.2 Creating a Batch File Using a Text Editor
      3. 3.7.3 Loading a Batch File
      4. 3.7.4 Adding a Batch File to the Firmware
    8. 3.8  Peripherals
    9. 3.9  Firmware
      1. 3.9.1 Adding or Removing Patterns from the Firmware
        1. 3.9.1.1 Deleting Images
        2. 3.9.1.2 Adding Images
        3. 3.9.1.3 Adding Both Images and Batch Files
    10. 3.10 Flash Device Parameters
    11. 3.11 JTAG Flash Programming
    12. 3.12 Intel (Altera) FPGA Programming
  5. 4Connectors
    1. 4.1 Input Trigger Connectors
    2. 4.2 Output Trigger Connectors
    3. 4.3 DLPC900 UART Headers
    4. 4.4 DLPC900 I2C Port 0
    5. 4.5 DLPC900 I2C Port 1
    6. 4.6 DLPC900 I2C Port 2
    7. 4.7 JTAG Boundary Scan
    8. 4.8 GPIO and PWM
    9. 4.9 Power
  6. 5Power Supply Requirements
    1. 5.1 External Power Supply Requirements
  7. 6Safety
    1. 6.1 Caution Labels
  8. 7Revision History

Peripherals

Click the Peripherals button at the top of the GUI to display the Peripherals panel as shown in Figure 4-19.

GUID-20201113-CA0I-PQNW-P9BS-8BW7JBWM7GN5-low.png Figure 3-19 Peripherals Panel
  • The I2C group box allows external I2C device to be controlled using one of the DLPC900 I2C interfaces. For example, if an LED driver requires I2C communications to enable the LEDs, then a command can be sent to the LED driver using this interface. When using the I2C interfaces, first configure the I2C port using the commands within the I2C Settings and then perform data transfers using the commands within the I2C Read/Write.
  • The Clock A Configuration group box allows the user to enable and control the output frequency of OCLKA. The clock can be used as a source to some external logic.
  • The GPIO Configuration group box allows the user to configure any of the nine available GPIOs. These GPIOs can be configured as inputs or outputs.
  • The Pulse Width Modulate Control group box allows a user to configure any of the four available PWM outputs.
Note:

GPIO_PWM_00 – GPIO_PWM_03 are shared GPIO\PWM outputs.