DLPU102B December 2020 – July 2022
The DLP LightCrafter DLPC900 GUI communicates with the DLPC900 using USB 1.1. The DLPC900 enumerates as a USB device with HID Support. The PC polls all the HID peripherals and once the PC detects the DLPC900, the Connected radio-button changes to green. If the USB cable is disconnected, the Connected radio-button changes to red. Once the Connected radio-button shows green, the firmware Version and the Tag name are displayed.
The Virtual Connection option is useful when there is no connection to the EVM. When the Virtual Connection is checked, all commands continue to operate as if there was a connection to the EVM except for firmware uploads and updating the Look Up Table (LUT).