1.7 DLP LightCrafter Dual DLPC900 EVM and DMD EVM
Assembly
The DLP Dual DLPC900 EVM requires a
suitable DMD EVM listed in Section 2.2.
The flex cables provided with
the DMD EVM have one end marked "DMD End" with key pins arranged diagonally
that only fit one way onto the DMD board preventing attachment to the wrong
side of the board. Place the insulated backer plate on the other side of the
DMD board from the flex side with connection pins and carefully tighten the
screws. Alternate tightening the screws from side to side until the screws
are firm, but not overtightened (SCREW TORQUE REQUIREMENT: 6-8 IN*LB
[0.7-0.9 N*m]). Figure 2-7shows the flex cable DMD ends correctly assembled to an
example DMD EVM board.
The other end of the flex
cables attach to the dual DLPC900 controller board. The key pins are
arranged laterally symmetric and can be inserted from either side of the
controller board. To ensure the cables are connected to the correct side of
the dual DLPC900 controller board, check that the connection flex pins are
facing the pads as shown in Figure 2-6. Place the insulated backer plate on the other side of
the controller board from the flex with pins and carefully tighten the
screws. Alternate tightening the screws from side to side until the screws
are firm, but not overtightened (SCREW TORQUE REQUIREMENT: 6-8 IN*LB
[0.7-0.9 N*m]). Figure 2-7 shows the flex cable ends correctly assembled to the
dual DLPC900 controller board.
Figure 1-6 DLPLCRC900DEVM Flex Cable Pads
Figure 1-7 Assembled
DLPLCRC900DEVM with DLPLCR90EVM