SBAA716 August 2025 DLP160AP , DLP160CP , DLP2000 , DLP230GP , DLP230KP , DLP230NP , DLP3010 , DLP3310 , DLP4710 , DLP472NE , DLP472TE , DLP472TP , DLP480RE , DLP550HE , DLP550JE , DLP650LE , DLP650NE , DLP650TE , DLP651LE , DLP651NE , DLP660TE , DLP670RE , DLP780NE , DLP780TE , DLP781NE , DLP800RE , DLP801RE , DLP801XE
Thanks to cutting-edge advancements, rainbow effect is nearly extinct. Modern 1-chip DLP® projectors boast sleek new designs, fast refresh rates and new illumination technologies like LED and RGB laser. These upgrades deliver crisp, smooth visuals with consistent colors, making rainbow artifacts a thing of the past.
Figure 1 Vibrant and Eye-Catching Image
With Unparalleled Color AccuracyThe rainbow effect is a brief color flash seen in some older DLP projectors that was more common in early lamp or older laser phosphor color wheel systems. Slower refresh rates in those models cause subtle color separation for certain viewers, especially in high-contrast or fast-moving scenes. Not everyone notices the rainbow effect, as it varies by individual perception. With laser phosphor projectors featuring enhanced color wheel designs or the use of newer illumination technology such as LED or RGB lasers, projector viewers enjoy a stunning, virtually rainbow-free viewing experience.
Newer categories of illumination can also be used with DLP technology. These illumination types remove the use of the color wheel:
Color overlap is supported in DLP projectors using LED or RGB laser illumination technology. Solid state LED or RGB laser illumination enables up to six times faster color switching when compared to earlier generation systems. This faster color refresh rate greatly reduces, or in our fastest color refreshing systems, can perceptually eliminate color breakup creating a DLP display viewing experience similar to what is found on TI DLP Cinema® systems. This much higher color refresh rate also enables much improved camera capture of the projected image which is an important use case.
In DLP projectors using laser phosphor, the color wheel is a critical component that spins to filter light into sequential red, green, blue and sometimes additional colors, like white or yellow, to create a full-color image. Improvements in color wheel design have been instrumental in reducing or eliminating this rainbow effect artifact. Here are the key advancements:
The latest DLP display controllers provide support for more color cycle with up to 20 cycles per color in a 60 Hz system. More color cycles in a projector reduce the rainbow effect because they cycle through the primary colors (red, green, blue) more rapidly, which reduces the amount of time the eye can perceive a single color being displayed, making the separation between colors less noticeable and diminishing the perceived rainbow effect.
Project an incredible portrayal without worrying about rainbow effect by using a DLP projector using the latest color wheel enhancement or an LED or RBG laser projector that provide color saturation and wide color gamut without using color wheels. The use of newer controllers and utilization of color overlap can also help to eliminate rainbow artifacts. Any of these solutions will deliver one of the best images in the industry.