SBASB60B October 2024 – August 2026 AMC0230S-Q1 , AMC0330S-Q1
PRODMIX
The AMC0x30S-Q1 provides a single-ended analog output voltage proportional to the input voltage. The output is referred to GND2 and is galvanically isolated from the input of the device. The output is designed to connect directly to the input of an ADC.
The mid-range output voltage is set by the REFIN pin. For any input voltage within the specified linear input range, the device outputs a voltage equal to:
The device is linear within the specified linear full-scale range. Beyond the linear full-scale range, the output continues to follow the input, but with reduced linearity performance. The output clips when the input voltage reaches the clipping voltage. Figure 7-2 shows the input-to-output transfer characteristic.