SBAU353 October 2021
Download the latest version of the EVM GUI installer from the Tools and Software folder of the ADS131A04EVM and run the GUI installer to install the EVM GUI software on your computer.
Manually disable any antivirus software running on the computer before downloading the EVM GUI installer onto the local hard disk. Depending on the antivirus settings, an error message may appear or the installer. The exe file can be deleted.
Accept the license agreements and follow the on-screen instructions shown in Figure 6-2 to complete the installation.
Figure 6-2 ADS131A04 Software
Installation PromptsAs a part of the ADS131A04EVM GUI installation, a prompt with a Device Driver Installation (as shown in Figure 6-3) appears on the screen. Click Next to proceed.
Figure 6-3 Device Driver Installation
Wizard PromptsA notice may appear on the screen stating that Windows cannot verify the publisher of this driver software. Select Install this driver software anyway.
The ADS131A04EVM requires the LabVIEW® run-time engine and may prompt for the installation of this software, as shown in Figure 6-4, if not already installed.
Figure 6-4 LabVIEW Run-Time Engine
InstallationVerify that C:\Program Files (x86)\Texas Instruments\ADS131A04EVM is after these installations.