SBAU356 September 2020
After pressing "Configure" within the ADC35xx GUI perform the following steps to setup HSDC pro:
Launch HSDC Pro
Select the TSW1400 and click OK
Figure 4-3 HSDC Pro: Connect to TSW1400. Click OK for the no firmware loaded prompt.
Select “ADC3660_2W_16bit_CMOS" to load firmware, and click Yes.
Figure 4-4 HSDC Pro ini file selection for
Bypass Mode. Click on the cog next to “ADC Output Data Rate”.
Figure 4-5 HSDC Pro Cog Wheel. Enter 25M within the box that says “ADC Sampling Rate”
Enter the input frequency of the input signal in the box that says "ADC Input Signal Frequency"
Enter 0 in the box that says "NCO"
Enter 1 in the box that says "Decimation"
Press okay
Figure 4-6 Bypass Mode HSDC Pro
Parameters. Press Capture
Figure 4-7 Bypass Mode Capture. The analog input signal power may need to be adjusted to reach -1 dBFS.