SBAU376A December 2021 – March 2022 TMAG5328
The TMAG5328 in this EVM can be powered from either the main power rail on the board, which is labeled as VCC on the board, or can be powered from an external power supply that is independent of the main power rail of the board. To power the TMAG5328 from the VCC rail, add a jumper on pins 1 and 2 of header J2. By adding the jumper to J2, the TMAG5328 is powered from the same power supply as the DAC43701. If the SCB is connected to the TMAG5328EVM, then the SCB provides 3.3V on VCC, so an external power supply must not be connected to VCC in this scenario. If the SCB is not connected to the TMAG5328EVM, however, then VCC can be connected to an external power supply by connecting the external power supply between the VCC and GND test points. In this scenario, the external power supply voltage must be set to somewhere within 1.8V to 5.5V, which is within the normal power supply voltage range of both the DAC43701 and TMAG5328.
To power the TMAG5328 from an external power supply that is independent of the board's main power rail, remove the jumper on J2 and connect J4 Pin 1 (labeled TVCC on the board) to the positive terminal of a power supply and then connect the ground of the board to the negative terminal of the power supply. This configuration enables powering the TMAG5328 from a different power supply than the DAC and the SCB. The TMAG5328 power supply voltage must be set to be within 1.65V to 5.5V, which is the normal power supply voltage range of the TMAG5328.
Various jumper headers and jumper settings are present to add to the flexibility to the board. Some of these headers require that jumpers be placed appropriately for the board to correctly function. Table 4-1 shows the functionality of each header on the board.
|
Header Name |
Type |
Main Functionality |
Valid Use-Cases |
|---|---|---|---|
|
J1 |
2 x 6 pin header |
Connection to SCB |
To connect the TMAG5328EVM to the SCB, connect this male header to the female J1 header on the SCB. The pin mappings on this header include the following (even pins are on the top row and odd pins are on the bottom row):
|
|
J2 |
2-pin jumper header |
PWR: TMAG5328 power select |
|
|
J3 |
3-pin jumper header |
Threshold Adjustment Option Selection |
|
|
J4 |
3-pin header |
Probe here for TVCC and GND. |
Probe here for TVCC (pin 1) and GND (pin 3). If a jumper is pressed on J2, TVCC is connected to VCC on the board. To power the TMAG5328 from an external power supply that is independent of VCC, remove the jumper header on J2 and connect the external bench power supply between TVCC and GND. |