SBAU394B April   2022  – August 2025

 

  1.   1
  2.   Description
  3.   Features
  4.   4
  5. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
    5. 1.5 Quick Start Guide
  6. 2Hardware
    1. 2.1 ADC Analog Input Signal Path
    2. 2.2 ADC Connections and Decoupling
    3. 2.3 Power Supplies
    4. 2.4 ADC Input Clock (CLK) Options
    5. 2.5 Digital-to-Analog Converter (DAC)
    6. 2.6 Digital Interface
    7. 2.7 Connection to the PHI
    8. 2.8 Digital Header
  7. 3Software Installation
  8. 4EVM Configuration and GUI Operation
    1. 4.1 EVM Configuration
    2. 4.2 GUI Operation
      1. 4.2.1 EVM GUI Global Settings for ADC Control
      2. 4.2.2 Register Map Configuration Tool
      3. 4.2.3 Time Domain Display Tool
      4. 4.2.4 Spectral Analysis Tool
      5. 4.2.5 Histogram Tool
      6. 4.2.6 DAC Configuration Tool
  9. 5Hardware Design Files
    1. 5.1 Schematics
    2. 5.2 PCB Layout
    3. 5.3 Bill of Materials
  10. 6Additional Information
    1. 6.1 Trademarks
  11. 7References
  12. 8Revision History

Quick Start Guide

The following instructions are a step-by-step guide to connecting the ADS1285EVM-PDK to the computer and evaluating the performance of the ADS1285:

  1. Review the default jumper settings in Section 4 and GUI software installation in Section 3.
  2. Connect the ADS1285EVM to the PHI. Install the two screws as indicated in Figure 1-1.
  3. Attach the micro USB to the PHI board and your PC. Three LEDs illuminate on the PHI board to indicate connectivity to the PC.
    1. LED D5 on the PHI lights up, indicating that the PHI is powered up.
    2. LEDs D1 and D2 on the PHI start blinking to indicate that the PHI is booted up and communicating with the PC. Figure 1-1 shows the resulting LED indicators.
      ADS1285EVM-PDK ADS1285EVM-PDK Hardware Setup and LED IndicatorsFigure 1-1 ADS1285EVM-PDK Hardware Setup and LED Indicators
  4. Launch the ADS1285EVM-PDK GUI software and power can be supplied to the EVM.
    1. The default installation path is C:\Program Files (x86)\Texas Instruments\ADS1285 EVM.
  5. As shown in Figure 1-2, use the Configuration section of the GUI for a specific clock input, desired data rate, and number of samples. Then, use the Capture button to collect data. Section 4.2.1 details the EVM GUI global input parameters and the various pages within the GUI.
    ADS1285EVM-PDK EVM GUI Global Input ParametersFigure 1-2 EVM GUI Global Input Parameters