SBAU431 July 2024 ADS1282
Figure 3-6 shows all connections to the ADS1282 data converter (U1). Each power supply connection has a pair of 10μF and a 1μF decoupling capacitors. Make sure these capacitors are physically close to the device and have a good connection to the AVSS plane. The supply connections also have a series 0Ω resistor. These resistors facilitate current measurement for the ADC. Each digital pin has a 49.9Ω series resistor. These resistors smooth the edges of the digital signals to provide minimal overshoot and ringing.