Figure 7-1 shows a circuit example of the LOG200 driving a
fully-differential input ADC. This circuit uses the auxiliary op amp in the
inverting configuration to perform a single-ended to differential conversion for
driving the ADS7954 fully-differential, SAR ADC.
Table 6-3 show the typical LOG200 specifications for error
calculation:
Design Notes:
- Select high-grade C0G (NP0) capacitors for
CDIFF, CCM1, CCM2 and CFB to
minimize distortion.
- Use 0.1% resistors for RIN and
RFB to minimize gain error and drift on the inverting amplifier
circuit.
- The R-C-R filter placed at the ADS7054 inputs
drives the SAR as a charge kickback filter. The filter component values depend
on the data converter sampling rate, the ADC sample-and-hold structure, and the
data converter requirements. The filter combination (RFIL and
CFIL) is tuned for ADC sample-and-hold settling performance while
maintaining amplifier stability. The component value selection is dependent on
the data converter sampling rate, the ADC sample-and-hold structure.
- The values shown in this example provide good
settling performance for the LOG200 and ADS7054 14-Bit, 1-MSPS, differential
input, SAR ADC. If the circuit is modified, the circuit designer can need to
select a different R-C-R filter depending on the ADC selection and application
needs. See the Introduction to SAR ADC Front-End Component Selection training
video for an explanation of how to select the RC filter for best settling
performance.