SBOS622D July 2018 – May 2025 OPA855
PRODUCTION DATA
There are two main approaches for current to voltage conversion. One uses a noninverting voltage feedback amplifier in combination with a shunt resistor to first convert current and then further amplify the optical signal. The other approach configures an amplifier for transimpedance applications which combines both steps into one. Figure 9-4 shows the standard configuration for both approaches.
Both configurations provide a low output impedance stage which provides the ability to interface with various types of loads. However, the noninverting option comes with a few disadvantages. The TIA input impedance is near zero, since the amplifier keeps the voltage at the inverting input node at the same potential as the non-inverting input node. While the VFB input impedance is equal to the shunt resistor RL. In the case of the VFB amplifier, the signal response can be slowed due to a large time constant created by the shunt resistor and capacitor. Also, the linearity of the photodetector can suffer, especially for higher detector currents due to the varying voltage bias produced at the shunt resistor. And, since the voltage bias of the photodetector is no longer constant for all detector currents, the diode’s internal capacitance can vary. Using a TIA, the voltage bias remains constant at the voltage set by the non-inverting node, and can provide level shifting to the signal which is especially useful for single-supply configurations.
OPA855 offers 8 GHz of gain bandwidth, high slew-rate, and low noise which makes this device an excellent for a wide range of photodetectors. Figure 9-5 shows the OPA855 configured as a transimpedance amplifier (TIA) in a wide-bandwidth, optical front-end system. Various types of optical sensors can be used as an optical input to the amplifier: photodiode (PD), avalanche photodiode (APD), photomultiplier tube (PMT), and multipixel photon counter (MPPC) or known as solid-state photomultiplier (SiPM). Optical detection applications have commonly used APDs, but ultra-low light source detection has been a challenge in past options. With technologies such as PMTs and MPPCs, the high intrinsic gain, while maintaining a fast output, requires a low noise, high-speed interface. The OPA855 can accommodate for these optical challenges and can work equally as well in these applications.
Transimpedance applications require low voltage and current noise for an excellent system performance. As a result of the high input impedance structure, the OPA855 has a great balance between low input-referred voltage noise and current noise that is consistent over frequency. Overall, the amplifier noise must have minimal impact to the total noise of the application. Examine the total input referred noise to the optical sensor.
Noise sources in optical sensors vary especially when introducing gain and photon paralleling. Optical power, gain, and applied reverse bias are the main characteristics that can affect signal to noise ratio. Standard photodiodes contribute the lowest noise at the highest quantum efficiency. Internal to photodiodes, noises sources include shot and thermal. Shot noise is a random occurrence of photodetection which arises in periods of both light and dark. Dark current is noise that occurs in the absence of an optical source which can be included with shot noise. And, thermal noise originates from the shunt resistance internal to the diode. At the lower signal levels, shot noise can dominate. Figure 9-6 shows an example of the noise sources present in a transimpedance amplifier circuit. The total TIA noise is the root sum square of each component within the system: photodiode noise, amplifier current noise, amplifier voltage noise, and feedback resistor noise.
Interfacing with APDs is similar to interfacing with PIN PDs, but APDs have additional noise factors due to the internal gain. APDs have increased shot noise and the addition of a multiplication excess noise factor. Decreasing capacitance, increasing diode shunt resistance, and decreasing reverse voltage bias applied to the APD deceases noise at the expense of response time. The MPPCs total noise is comparable to APDs, but with differing noise sources. This optical sensor includes digital-like noise factors such as dark count rate, after pulsing, and optical crosstalk due to the parallel gain cells. For PMTs, dark count rate is lower. In general, PMT total noise is comparable to PDs with an internal gain comparable to APDs. However, PMTs have the lowest quantum efficiency of the optical sensor space.