SBVA094A February   2025  – July 2025 TPS7A21

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Oscilloscope Basics
  5. 2Implications of Parasitics
  6. 3Common Oscilloscope Issues
    1. 3.1 Choosing an Oscilloscope Probe
    2. 3.2 Sufficient Sampling
    3. 3.3 Visualization
    4. 3.4 Measuring Currents Using Current Probes
    5. 3.5 Bandwidth Limiting and Averaging
  7. 4Parasitic Effects on Common Measurements
    1. 4.1 Load Transients
    2. 4.2 Power Supply Rejection Ratio
    3. 4.3 Output Noise Voltage
  8. 5Summary
  9. 6References
  10. 7Revision History

Bandwidth Limiting and Averaging

Bandwidth limiting and averaging can be useful tools to reduce the amount of noise in a measurement, but must be used with caution. Both of these tools have advantages if used appropriately, but can give false impressions if used without consideration of the measurement being taken.

Although bandwidth limiting significantly reduces high-frequency noise present in a waveform, bandwidth limiting can also attenuate or filter components of the waveform that are important to see for debug, such as overshoot and undershoot. This can lead to inaccurate measurement readings, as seen in Figure 3-13 and Figure 3-14. If there are no expected high-frequency components in the intended measurement, bandwidth limiting can be used to get a clearer picture of the electrical behavior of the circuit with less noise, but in some cases there are unexpected high-frequency signals due to noise coupling or resonances from underdamped filters or parasitics. We recommend starting with full bandwidth and only limit the bandwidth after some confidence has been developed that the measurement does not have important high-frequency components.

 Full Bandwidth (500MHz)
                        Rising Edge SignalFigure 3-13 Full Bandwidth (500MHz) Rising Edge Signal
 Bandwidth Limited (20MHz) Rising Edge SignalFigure 3-14 Bandwidth Limited (20MHz) Rising Edge Signal

Averaging can be a useful tool when there is no easy way to reduce noise through long measurement wires. This method requires that the waveform to be measured is consistent between measurements. Figure 3-16 shows how the noise in the measurement shown in Figure 3-15 is reduced by averaging 5 samples on the load transient shown on Channel 3.

 Load Transient with No
                        AveragingFigure 3-15 Load Transient with No Averaging
 Load Transient with 5
                        Sample AverageFigure 3-16 Load Transient with 5 Sample Average