SCPS286A July 2025 – February 2026 TPLD2001
PRODUCTION DATA
The outputs of this macro-cell act as virtual inputs into the device. The routing of the signal into the Connection Mux is shared with the physical digital input pins, so if a virtual input is used, the digital input pin resource is no longer available and the Connection Mux input is sourced from the Virtual Input register. Table 8-35 shows the shared resource between the digital input pin and the virtual input.
Virtual input | VIR_IN0 | VIR_IN1 | VIR_IN2 | VIR_IN3 | VIR_IN4 | VIR_IN5 | VIR_IN6 | VIR_IN7 |
Digital input pin | IO1 | IO2 | IO3 | IO4 | IO5 | IO6 | IO7 | IO9 |