SCPS286A July 2025 – February 2026 TPLD2001
PRODUCTION DATA
The state machine macro-cell has 26 inputs from the connection mux: 24 state transition inputs, 1 clock input, and 1 reset input.
Each of the 24 state transition inputs are active-high inputs, meaning a high-level input would trigger a state transition given the timing considerations are met. Further, these 24 inputs are grouped such that each set of 3 inputs drives a transition into a particular state. For example, there are 3 inputs that drives a transition from any state into State 2. Thus, this limits the maximum number of transitions into a particular state to 3.
When operating the state machine in synchronous mode and a state transition condition is met, the state transition will occur on the next rising edge of the clock input. In asynchronous mode, when a state transition condition is met, the state transition occurs asynchronously and the clock input is unavailable/ignored.
There is also an active-low, asynchronous reset input which, when asserted, puts the state machine into a reset state and, when released, will place the state machine in the user-selected initial state.