SCPS286B July 2025 – July 2026 TPLD2001
PRODUCTION DATA
When configured as an Edge detector (EDET), this macro-cell generates a pulse of approximately 20ns width when a valid edge is detected. The edge on which the Edge detector generates a pulse is determined by the Edge select parameter and can be configured as:
Rising: only rising edges of IN generate a pulse.
Falling: only falling edges of IN generate a pulse.
Both: both rising and falling edges of IN generate a pulse.
Figure 8-20 shows an example of how the EDET macro-cell operates with respect to the Edge select parameter.