SCPS299A May 2025 – September 2025 TXE8116-Q1 , TXE8124-Q1
ADVANCE INFORMATION
In Burst Mode Read Transactions, the initial address is specified by the controller device and sent to the peripheral. For subsequent accesses, the address is automatically incremented to the next valid address (second address byte) corresponding to the next port. This automatic address increment continues as long as the CS remains active low and SCLK pulses are received by the peripheral device.
The burst mode transaction continues sequentially, automatically advancing the address for each valid port address, until the last port address is reached for the specified feature (first address byte). Once the last valid port address is reached, the peripheral will output all 0s from SDO, indicating the end of the valid data sequence.
It is important to note that Burst Mode will not automatically increment to a new feature address after reaching the last port address of a given feature. The controller must manually specify the new feature address if needed for further transactions.