SDAA059 September 2025 TMCS1123 , TMCS1123-Q1 , TMCS1126 , TMCS1126-Q1 , TMCS1127 , TMCS1127-Q1 , TMCS1133 , TMCS1133-Q1 , TMCS1143 , TMCS1148
Correct selection of solder paste is required when using larger pads for the mitigation of solder voiding in larger solder joints. In general, a no-clean solder paste is a preferred option to optimize these joints for best performance.
In general, there are little to no risks in the use of an SOIC-10 package on an SOIC-16 footprint. Across all examinations, there is little to no observed change in device thermal performance, PCB substrate integrity, or device leadframe integrity after 1000 hours of continuous temperature stress.