SDAA080 September 2025 TPS2HCS08-Q1 , TPS2HCS10-Q1
OL_ON mode can be enabled by setting the relevant OL_ON_EN_CHx bit high in the respective CHx_CONFIG register. For the device to accept the command and enter OL_ON mode, the output current must be below the IENTRY_OL_ON threshold. If the output current is not, then the device does not enter OL_ON mode and OL_ON_EN_CHx stays low. If the output current is below IENTRY_OL_ON and OL_ON_EN_CHx is set high, then KSNS decreases and FET ON resistance increases as specified above until OL_ON_EN_CHx is set low or the output current exceeds IEXIT_OL_ON.
To enable the 8x ADC input scaling, set the ISNS_SCALE_CHx bit and the respective CHx_CONFIG register high. There is no other requirement to enable ADC input scaling.
During OL_ON mode and ADC input scaling operation, TI recommends that the MCU periodically check OL_ON_EN_CHx to make sure the device is still in OL_ON mode. When reading the respective channel current sense, the ISNS_SCALE_EFF_CHx bit is included in the ADC_RESULT_CHx_I current sense result register to notify the MCU of what multiplier to use to read the current sense result. This bit directly shows whether a 1x or 8x ADC scaling factor is used.
Figure 3-1 OL_ON Enable Flowchart