SDAA088 September   2025 AMC0100R , AMC0311R , AMC0311R-Q1 , AMC0330D , AMC0330R , AMC0330R-Q1 , AMC0330S , AMC0336

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Pairing Ratiometric Output Isolation Amplifier With ADC
    1. 2.1 Test Setup
    2. 2.2 REFIN Voltage Tracking
    3. 2.3 Ratiometric Configuration Noise Rejection
    4. 2.4 Spurious-Free Dynamic Range
    5. 2.5 Transient Response of REFIN to VOUT
    6. 2.6 Transfer Function of REFIN to VOUT
  6. 3Summary
  7. 4References

Spurious-Free Dynamic Range

The spurious-free dynamic range (SFDR) is more relevant parameter in the communication industry, but this is also a practical indicator that can be clearly seen in the frequency domain (Figure 2-6). This parameter helps in understanding how significant the injected noise is compared to the signal of the interest.

 Spurious-Free Dynamic
                    Range Figure 2-6 Spurious-Free Dynamic Range

The test procedure and the configuration are similar to those in the previous example, but not identical. The input voltage VIN is a 10kHz sinewave with 2VPP amplitude. This signal represents the signal of the interest. The AWG injects a modulated VREF, as in the previous example.

Figure 2-7 shows SFDR performance of the ratiometric configuration compared to the non-ratiometric configuration. The default non-ratiometric configuration dynamic range, which is determined by the ratio between the injected noise and the signal of interest, remains practically constant.

 Spurious-Free Dynamic Range
                    Comparison Between the Fixed Gain and Ratiometric Configuration Figure 2-7 Spurious-Free Dynamic Range Comparison Between the Fixed Gain and Ratiometric Configuration