SFFS624B March 2024 – August 2025 MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
There is one window comparator unit available in the ADC that can be used to check if the input signal is within the predefined threshold values set by software. The ADC result (digital value corresponding to the input signal level) that goes into MEMRES or FIFO is what gets checked against the threshold values of the window comparator.
Based on the comparison, the window comparator can generate 3 interrupt conditions:
The window comparator low and high threshold values are global for all channels and the window comparison feature can be enabled for each channel, as needed, using the WINCOMP bit in the MEMCTL register.
When the ADC result data format (CTL2.DF) or resolution (CTL2.RES) configuration is changed, the window comparator threshold values are not reset by hardware and are retained as is. The software application is expected to reconfigure the threshold values as appropriate after changing the data format and resolution configuration.