SFFS700 May 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
The standardized E-GAS monitoring concept (6) for engine management systems generated by the German VDA working group “E-Gas-Arbeitskreis” is an example of a well-trusted safety-architecture that may be used for applications other than engine management systems provided it fits the purpose of the new application in terms of diagnosis feasibility, environment constraints, time constraints, robustness, and so forth (7). For more information, see Figure 4-4.
Figure 4-4 E-GAS
System Overview From StandardThe TMS320F28P65xD/S MCU device family supports heterogeneous asymmetric architecture and their functional safety features lend themselves to an E-GAS concept implementation at system level as indicated in Figure 4-5. In the first level (Level 1), the functions required for the system mission are computed. Second level (Level 2) checks the correct formation in first level based on selected set of parameters. Third level (Level 3) implements an additional external monitoring element, for the correct carrying out of the mission in the first level and/or monitoring in the second level. The exact functional safety implementation and the modules used for realizing Level 1 and Level 2 and the external monitoring device for realizing Level 3 are left to the system designer. Though Figure 4-5 indicates CLA implementing Level 1 and CPU(28x) implementing Level 2 of the EGAS monitoring concept, both the processing units are capable of implementing either of the levels. The application can determine the partitioning based on the system requirements.
Figure 4-5 VDA E-Gas Monitoring Concept
Applied to C2000 MCU