SLAA635A September   2024  – August 2025 MSPM0G3507

 

  1.   1
  2. Description
  3. Required Peripherals
  4. Design Notes
  5. Design Steps
  6. Device Configuration
  7. Design Considerations
  8. Reference
  9. E2E
  10. Trademarks
  11. 10Revision History

Design Considerations

  1. Voltage reference:
    • Vref is set to GND in this example but a voltage can be connected to R4 to change the DC level.
  2. Output limitation:
    • For the MSPM0 family, the output signal cannot be greater than VDD.
  3. The PGA built into the OPA module can be used as well, but the external resistor values need to be adjusted. The ratios are not necessarily going to be equal; therefore, matching can be imperfect.
  4. The ADC can be set for different sampling speeds and conversion resolutions as described. These configurations can be done in SysConfig and more details on the capabilities of the ADC and OPA are found in the device TRM and data sheet.
  5. LaunchPad Configuration: On the LaunchPad, the OPA inputs and outputs can be connected to different circuitry such as the onboard photodiode or thermistor circuits. Check the associated LaunchPad user guide to determine which jumpers to remove.