SLAA638A august 2014 – may 2023 MSP430I2040 , MSP430I2041
After the calibration of VGAIN, IGAIN and PGAIN, use the following steps to calibrate the compensation to wire resistance and EMI capacitance.
Calibrating RES:

where,
RWIRE is the estimated resistance
VREF(Imax) is the reference meter voltage reading at the current set for IGAIN calibration
VUUT(Imax) is the unit under test voltage reading at the current set for IGAIN calibration
Imax is the current set for IGAIN calibration
Or, if percentage of error is used (as with the provided calibration software):
Calibrating CAP:

where,
C is the estimated EMI filter capacitance
V is the voltage set for calibration of C
PAPPERANT_REF is the apperant power reading of the reference meter at the setting for this calibration
PAPPERANT_UUT is the apperant power reading of the unit under test at the setting for this calibration
PACTIVE is active power reading of the reference meter
(suppose already calibrated to be the same as active power reading of UUT):