SLAAE76C March 2023 – May 2025 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507
The MSPM0G OPA is a zero-drift chopper stabilized operational amplifier with a programmable gain stage. The OPA can used for signal amplification and buffering and can work in general-purpose mode, buffer mode and PGA mode.
When using the OPA in general-purpose mode, add an external resistor and capacitor to create the amplifier circuit. The OPA can be configured through software for buffer mode. For PGA mode, software can configure the OPA up to 32x PGA gain.
When two or more OPAs are available on a device, the two can be combined to form a differential amplifier. The output equation for the differential amplifier is given by the Vdiff equation in Figure 6-2.
Alternately, two or more OPAs that are available on a device can be combined to form a multistage or cascaded amplifier. Using the programmable input muxes, all combinations of inverting and non-inverting multistage amplifiers can be implemented. The output equation for the noninverting to noninverting cascaded amplifier is given by the Vout equation in Figure 6-3.