SLAAE88D December   2022  – September 2025 MSPM0C1105 , MSPM0C1106 , MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507 , MSPM0H3216 , MSPM0L1105 , MSPM0L1106 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Introduction
    1. 1.1 Bootloader Concept
    2. 1.2 MSPM0 Bootloader Structure
      1. 1.2.1 ROM-Based BSL
      2. 1.2.2 ROM-Based BSL With Flash-Based Plug-In Interface
      3. 1.2.3 Flash-Based Secondary BSL
    3. 1.3 MSPM0 BSL Features and Demos Summary
  5. 2BSL Host Implementation Summary
  6. 3BSL Configuration in Non-Main (Configuration NVM)
    1. 3.1 Non-Main Introduction
    2. 3.2 Example – Disable PA18 BSL Invoke Pin With Sysconfig
  7. 4Bootloader Host
    1. 4.1 MCU Host Code Introduction
      1. 4.1.1 Hardware Connection
      2. 4.1.2 TXT to Header File Conversion
      3. 4.1.3 Step-by-Step Using the Demo
    2. 4.2 PC Host Example
      1. 4.2.1 Prepare the Image File and Password File
      2. 4.2.2 Steps to Using the GUI
  8. 5Bootloader Target
    1. 5.1 Default ROM-Based BSL
      1. 5.1.1 UART Interface
      2. 5.1.2 I2C Interface
    2. 5.2 Flash-Based Plug-In Interface Demos
      1. 5.2.1 UART Interface
        1. 5.2.1.1 Step by Step Using the Demo
        2. 5.2.1.2 How to Debug the Plug-In Interface Code
      2. 5.2.2 I2C Interface
      3. 5.2.3 SPI Interface
      4. 5.2.4 CAN Interface
    3. 5.3 Secondary BSL Demo
      1. 5.3.1 Flash-Based Secondary BSL Start From 0x1000
      2. 5.3.2 Flash-Based Secondary BSL Start From 0x0000
        1. 5.3.2.1 Flash-Based 0x0 Address BSL Demo for MSPM0C
        2. 5.3.2.2 Live Firmware Update
  9. 6Common Questions
    1. 6.1 Linker File Modification
    2. 6.2 Factory Reset by CCS to Recover Device
  10. 7References
  11. 8Revision History

Steps to Using the GUI

  1. Connect the target device and the XDS110 to the PC. When using the XDS110 integrated in the LaunchPad kit, connect the micro USB cable to the PC as Figure 4-7.

    The ROM-based BSL UART pins for MSPM0G3507 are PA10 and PA11, and the pins are directly connected to the XDS110 backchannel UART, so all of the jumpers in J101 are required (see Table 4-7).

    On the LP-MSPM0L1306, the XDS110 backchannel UART pins are different from the BSL UART pins, so disconnect TXD and RXD in J101 and use jumper wires to connect PA22 and PA23 (see Table 4-7).

     LaunchPad Kit Connection
                        (Left: LP-MSPM0G3507, Right: LP-MSPM0L1306) Figure 4-7 LaunchPad Kit Connection (Left: LP-MSPM0G3507, Right: LP-MSPM0L1306)
    Table 4-6 Jumpers Connection
    Boards Mode Jumpers Need Populated Jumpers Need Unpopulated
    LP-MSPM0G3507 Target J101 (power, UART pins, Reset and BSL invoke pin), J4, J7(LED), J21, J22 (UART to J101 XDS) NA
    LP-MSPM0L1306 Target J101 (GND, 3V3, NRST, BSL), J2, J3(LED) J101 (TXD, RXD)

    For standalone XDS110, the auxiliary interface (AUX) uses the signal connections in Table 4-7.

    Table 4-7 Standalone Signal Connection
    Signal Standalone XDS110 Target Device
    Signal AUX Port Signal LP-MSPM0G3507 LP-MSPM0L1306
    NRST IO output IOOUT0 NRST NRST pin NRST pin
    Invoke IO output IOOUT1 Default: Invoke pin PA18 PA18
    UART RXD UARTRX TXD PA10/UART0_TX PA23/UART0_TX
    TXD UARTTX RXD PA11/UART0_RX PA22/UART0_RX
  2. Use the GUI to download the image to the target.
    1. Choose the TI-TXT format image file that need to be downloaded. (There are two demo images in the folder named input)
    2. Choose the TI-TXT format password file (a default file is in the input folder). For details on preparing this file, see Section 4.2.1.
    3. Choose hardware bridge.
    4. Click the download button.

      The GUI automatically invokes the BSL so there is no need to manually invoke the BSL during this operation.

     Steps to Download Image by
                        GUI With UART Figure 4-8 Steps to Download Image by GUI With UART
  3. If using the XDS110, this GUI supports XDS110 firmware version firmware_3.0.0.20 or higher. If errors occur when download the image, update the XDS110 firmware.
     Update XDS110
                        Firmware Figure 4-9 Update XDS110 Firmware