SLAAEH8 October 2024 AFE781H1 , AFE782H1 , AFE881H1 , AFE882H1 , DAC8740H , DAC8741H , DAC8742H
Similar to the previous test, this test measures the HART signal band through a filter. Here, the HCF_TOOL-31 filter is used. This filter is a 500Hz to 10kHz bandpass filter that allows all of the in-band HART signal through. The test is devised to view the noise when the HART signal is inactive and verify there is no in-band noise that can be received as a HART signal in error. Figure 3-13 shows the test setup for the output noise during silence.
Figure 3-14 shows the oscilloscope shot of the measurement of the output noise during silence. This shows the inactive HART signal at the top of the oscilloscope plot after the HART has been disabled. The middle trace in the plot shows the same signal filtered through the HCF_TOOL-31, showing the in-band noise for the primary variable. The bottom trace of the oscilloscope plot is the RTS which is high indicating the HART is inactive. Table 3-4 shows the results of the noise measured during silence.
| TEST | MEASUREMENT | MAXIMUM | RESULT |
|---|---|---|---|
| Broadband noise without filter | 2.08mVRMS | 138mVRMS | Pass |
| In-band noise using HCF_TOOL-31 bandpass filter | 3.23RMS | 22mVRMS | Pass |