SLAAEQ4 July   2025 MSPM0G1106 , MSPM0G1107 , MSPM0G1506 , MSPM0G1507 , MSPM0G1518 , MSPM0G1519 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1

 

  1.   1
  2.   Trademarks
  3. 1Introduction
    1. 1.1 Features Supported
    2. 1.2 CAN Frame Format
    3. 1.3 SPI Message Frame Format
  4. 2Implementation
    1. 2.1 SPI Message Format
      1. 2.1.1 SPI Commands
      2. 2.1.2 Instruction Set
    2. 2.2 Timeout Feature
    3. 2.3 Error Indication
    4. 2.4 Busy Status Indication
    5. 2.5 Message RAM Configuration
    6. 2.6 Test Environment
  5. 3References

Error Indication

An error is generated in the below conditions:

  • When instruction received by the Bridge device is not valid (received instruction opcode is not included in the list of instructions).
  • When offset address received by the bridge is not valid (received offset address not related to any of the CAN register address).

External SPI controller can use Read receive status instruction to check Error indication for the previous instruction.