SLAU723A October 2017 ā October 2018 MSP432E401Y , MSP432E411Y
CAN New Data 1 (CANNWDA1), offset 0x120
CAN New Data 2 (CANNWDA2), offset 0x124
The CANNWDA1 and CANNWDA2 registers hold the NEWDAT bits of the 32 message objects. By reading these bits, the CPU can check which message object has its data portion updated. The NEWDAT bit of a specific message object can be changed by three sources: (1) the CPU via the CANIFnMCTL register, (2) the message handler state machine after the reception of a data frame, or (3) the message handler state machine after a successful transmission.
The CANNWDA1 register contains the NEWDAT bits of the first 16 message objects in the message RAM; the CANNWDA2 register contains the NEWDAT bits of the second 16 message objects.
CANNWDAn is shown in Figure 11-21 and described in Table 11-24.
Return to Summary Table.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | NEWDAT | ||||||||||||||||||||||||||||||
| R-0x0 | R-0x0 | ||||||||||||||||||||||||||||||