SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
A DMA route is a fixed route between a peripheral and the DMA controller, which optionally has additional side-band signals to pass a DMA done condition from the DMA controller back to the triggering peripheral to indicate when a DMA activity has run to completion. The DMA trigger route is shown in Figure 7-2.
Most peripherals capable of generating a DMA trigger have an additional set of event management registers (in addition to the CPU_INT registers used for the CPU interrupt and any GEN_EVENTx generic route publishers). These registers can be used to select which peripheral condition to use for generating the DMA trigger.
When a trigger is received by the DMA, the DMA acknowledges the request and the peripheral clears the request. The DMA also acknowledges the cleared request, after which a new request can be asserted by the peripheral.
The DMA route can also contain status signals (for specific peripherals) to indicate to the triggering peripheral that a DMA transfer sequence has completed. For example, the DMA can be set up to transfer N number of bytes from an SRAM buffer into the UART TX data register based on the UART TX DMA trigger. Upon each trigger from the UART, the DMA will acknowledge that the transfer was successful. On the Nth byte, the DMA will send a complete status signal to the UART, which the UART can use to propagate a transfer completion interrupt to the CPU.
Certain peripherals (for example, the 12-bit DAC) do not implement an event management register set for managing their DMA triggers. In these cases, the peripheral implements specific DMA configuration logic such that the management registers are not needed to interface with the DMA. Figure 7-3 shows the model when the event management registers are not implemented. See the peripheral-specific section of this document for guidance on how to configure DMA channels in this case.