SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
The comparator compares the analog voltages at the positive (+) and negative (–) input terminals. If the + terminal is more positive than the – terminal, the comparator output is high. The polarity of the comparator output can be configured by using the OUTPOL bit in COMPx.CTL1 register. The comparator can be switched on or off using ENABLE bit in COMPx.CTL1 register. The comparator should be switched off when not in use to reduce current consumption. When the comparator is off, OUT is low when OUTPOL bit is set to 0, and OUT is high when OUTPOL bit is set to 1.
The comparator can be configured in fast or ultra-low-power mode using MODE bit in COMPx.CTL1 register. The default value of MODE bit is 0 which configures the comparator in fast mode. When MODE bit is set to 1 the comparator is configured in ultra-low-power mode. In the fast mode the comparator consumes higher current but the response time is faster. In the ultra-low power mode the comparator consumes very low current but response time is slower. To optimize current consumption for the application, the power mode that meets the comparator speed requirements should be selected (please see the device-specific data sheet for the comparator propagation delay).
The clock control for comparator is managed by System Controller (SYSCTL), SYSCTL knows if comparator module is enabled and it also knows if it is in ultra-low-power mode or fast mode. User needs to ensure the proper bus clock is selected for different comparator operation mode: